2024-09-06 02:53 AM
Hi.
I did "HSE on-board oscillator from X3 crystal (not provided)" on um1974-stm32.
But stlink doesn't recognize my board. Why?
I used an ats49 8Mhz 18pF crystal since there is no recommended crystal. C37 and C38 have 18pF attached.
HSE on-board oscillator from X3 crystal (not provided)
– SB148 and SB163 OFF
– SB8 and SB9 ON
– C37 and C38 soldered with 4.3 pF capacitors
– SB112 and SB149 OFF
2024-09-06 02:59 AM
STM32F7 not powered, not running?
2024-09-06 03:05 AM
I turned it on and tested it, but it's the same.
The below message is CubeIDE error messages.
STMicroelectronics ST-LINK GDB server. Version 7.8.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
2024-09-06 05:18 AM
Hi.
I'm pretty sure that board is dead.
I have another board that is identical so I tested it further.
As above, I added the 8MHz oscillator and capacitor according to the manual.
And I set the RCC and clock configuration as follows:
And I checked the program download and operation through stlink.
But when I downloaded again via stlink, my cubeIDE did not recognize stlink.(It does not mean that the nucleo board is not recognized.)
I disconnected the 8MHz oscillator again, and cubeIDE recognized the nucleo board via stlink.
Why is stlink not recognized when I operate the 8MHz oscillator?
Does the HSE frequency affect the SWD frequency? Help me!!!
2024-09-06 05:19 AM
The issue is not related to the oscillator. It doesn't need an oscillator to connect.
How confident are we that those connections are solid and correct? Hard for me to see on the board where the wires are attached.
2024-09-06 05:28 AM
I checked again all modified point on the Nucleo board.
I proceeded according to the manual(um1974-stm32).
------------------------------------------
- HSE on-board oscillator from X3 crystal (not provided): for typical frequencies and
its capacitors and resistors, refer to the STM32 microcontroller datasheet and to the
Oscillator design guide for STM8S, STM8A and STM32 microcontrollers Application
note (AN2867) for the oscillator design guide. The X3 crystal has the following
characteristics: 8 MHz, 8 pF, 20 ppm. It is recommended to use NX3225GD-8.000MEXS00A-
CG04874 manufactured by NIHON DEMPA KOGYO CO., LTD. The
configuration must be:
– SB148 and SB163 OFF
– SB8 and SB9 ON
– C37 and C38 soldered with 4.3 pF capacitors
– SB112 and SB149 OFF
------------------------------------------
I downloaded the code to run HSE via stlink with the 8M oscillator not running. And when I tried to download again, cubeIDE did not recognize the stlink.
2024-09-06 06:01 AM
See if you can connect with standalone STM32CubeProgrammer. Try holding BOOT0 high during reset.
2024-09-06 06:57 AM
Ok, but what's actually wired up here? Describe, don't just post pictures.
Common Ground between board pieces?