2021-02-24 1:33 PM
Attached please is the connected equipment, installed software and the error message.
Solved! Go to Solution.
2021-02-24 1:39 PM
Doesn't look like you have an ST-LINK/V2, and it's not plugged into the 20-pin header
2021-02-24 1:39 PM
Doesn't look like you have an ST-LINK/V2, and it's not plugged into the 20-pin header
2021-02-24 2:21 PM
Hi Tesla,
Sure, i do not have the ST-LINK/V2. Thanks for the info.
2021-03-01 8:52 AM
Dear Sirs!,
Did purchase ST-LINK/V2 but even after the upgrade being successful, still i can't connect the set up. Kindly advice.
Attached please are the photos of my set up for reference.
NB: All the four sensor lights are blinking continuously. I do have only one measuring sensor connected to the set up.
Thank you.