2023-04-15 03:36 PM
I cannot find the logic in the schematics about the mapping of the 2 stmod+ connectors.
Which pins of the stmod+ correspond to the MCU pins ?
Page 7 of the schematic folio is very confusing.
I just found pin 3 & 4 of the stmod+2 to be mapped to PG10 & PG9
Solved! Go to Solution.
2023-04-16 02:20 PM
This is perhaps more understandable if you look at it together with UM2839, section 7.12.
In the schematics of the board on page 7, however, everything is actually listed neatly:
etc.
And PA0 and PA4, for example, can then be found on page 3 on the STM32U585AII6QU, like all the other pins.
Does it answer your question?
Regards
/Peter
2023-04-16 02:20 PM
This is perhaps more understandable if you look at it together with UM2839, section 7.12.
In the schematics of the board on page 7, however, everything is actually listed neatly:
etc.
And PA0 and PA4, for example, can then be found on page 3 on the STM32U585AII6QU, like all the other pins.
Does it answer your question?
Regards
/Peter
2023-04-17 01:21 AM
Dear Peter,
Thank you - the perfect example of the guy not reading the user's manual till the end...
I focused only on the schematics, for sure the Stmod+ tables in the UM are more helpful to know which pin is wired to the MCU
Kind regards,
Jerome