2023-01-04 3:37 PM
It seems a silly question but we couldn't find the specification of the 15-pin connectors on NUCLEO-32. We have looked the user's manual, schematic and BOM. The only things we knew is they look like double-sided header from the pictures, they are .100" pitch from the drawing in user's manual, and they are ATOM PH254015B-09303 in BOM. We don't know and couldn't find who are ATOM and what the p/n PH254015B-09303 is about. We need more information of these connectors such as the formal drawing, datasheet and specs when we try to use NUCLEO-32 in our application. Can somebody help? Thanks.
-WQ
2023-01-05 12:29 AM
15 pin ? the arduino conn. ?
se schematics...STM32 Nucleo (32 pins) schematics
https://www.st.com/en/evaluation-tools/nucleo-l432kc.html#cad-resources
+
When your question is answered, please close this topic by choosing Select as Best.