2023-03-19 01:04 PM
2023-03-20 03:22 AM
You can find the explanation in UM1724, section 6.3.1, where JP1 refers to this, even if the network name PWR_EXT is not explicitly mentioned.
Does it answer your question?
Regards
/Peter
2023-03-20 03:22 AM
You can find the explanation in UM1724, section 6.3.1, where JP1 refers to this, even if the network name PWR_EXT is not explicitly mentioned.
Does it answer your question?
Regards
/Peter
2023-03-21 12:57 PM
oh so its a current limit from the USB Source interesting ill tell ya coming from arduino to stm32 is like minor league to professional lol
2023-03-21 01:01 PM
Yes, there are a few more things to consider, but this is made somewhat easier by tools such as STM32CubeMX.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-03-21 01:20 PM
i have another question it might be a bug actually i posted it its about debug the sfr tab is missing some registers in rcc apb2enr
2023-03-22 08:21 AM
You probably mean the question asked in this thread?
This is already in progress.
Regards
/Peter
2023-03-27 01:14 AM
lol thats me that asked that sorry im a forum noob