cancel
Showing results for 
Search instead for 
Did you mean: 

What happens if VBAT is higher than VDD?

Pahul_Singh
Associate II

Hello STM32 Folks,

I was hoping to get some information regarding VBAT on STM32U5 MCU. I am currently powering the STM32U5 MCU with 1.8V (VDD supply). I need to have external clock oscillator for the Real Time Clock that is powered by VBAT (Coin Cell battery 3.0V). The external clock oscillator can be powered by 1.65V to 3V.

I didn't find any information regarding VBAT being higher than VDD. Will there be any issue with 3.0 V levels for the external clock oscillator for RTC? Or do I need to regulate the VBAT voltage to 1.8V for external clock oscillator? 

Thanks,

3 REPLIES 3
SofLit
ST Employee

Hello @Pahul_Singh ,

According to the datasheet there is no constraint regarding this point VBAT vs VDD:

SofLit_0-1736270501125.png

VBAT max = 3.6V and not VDD.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Thanks for the fast response.
Pin PC14 on the STM32U5 device is the 32.768 KHz Oscillator input pin. This pin has the external oscillator powered by 3.0V connected to it. 

If the STM32 device is powered by 1.8V (VDD power supply), the logic voltage levels that the PC14 will accept are 0 to 1.8V. 
Is my assumption correct for this? 

Or the voltage levels that PC14 accepts are based on the VBAT pin.

Uwe Bonnes
Principal III

PC13/14/15 are powered by VBAT. If you have an external oscilator to PC14, you should power the oscillator from VBAT.