cancel
Showing results for 
Search instead for 
Did you mean: 

What are the BOR levels for STM32G030 ?

Akoli.2
Associate III

Hello!

When I connect to STM32G030 with the ST-Link programmer in the Options bytes tab, I can adjust the BOR levels (level 1-4 F and R). These levels are not described in the datasheet (DS12991 Rev 3). What are these levels and where can I find their descriptions?

1 REPLY 1
TDK
Guru

The STM32G0x0 doesn't have a BOR per the reference manual or the datasheet.

The STM32G0x1 does, and you can find the levels in the datasheet.

0693W00000HoJEoQAN.png 

If the BOR option bytes are available in STM32CubeProgrammer for the G0x0, they may or may not work the same as the G0x1. They may be available but simply not tested.

If you feel a post has answered your question, please click "Accept as Solution".