cancel
Showing results for 
Search instead for 
Did you mean: 

Using the st-link CLI

rokasjsutkus
Associate II
Posted on November 16, 2016 at 10:18

Hey,

After entering anything to the command line, it just goes off, doesn't do anything, tried different combinations, commands, anything, but it just exits and nothing. Dis anyone had similar problems, or knows whats wrong, or tell me that I'm using it wrong.

Thanks in advance.

#st-link-cli
3 REPLIES 3
slimen
Senior
Posted on November 16, 2016 at 12:00

Hello,

Which ST_LINK_CLI version are you using?

Have a look to the STM32 ST-LINK utility command line interface (CLI) section in the

http://http://www.st.com/content/ccc/resource/technical/document/user_manual/e6/10/d8/80/d6/1d/4a/f2/CD00262073.pdf/files/CD00262073.pdf/jcr:content/translations/en.CD00262073.pdf

User manual. Hope this helps you.

Regards

rokasjsutkus
Associate II
Posted on November 17, 2016 at 13:01

The version is 2.5.0

I have read the manual, but it doesn't mention anything about the CLI closing it self just by writing a command, or anything at all.

rokasjsutkus
Associate II
Posted on November 17, 2016 at 13:47

Problem solved, reinstalled the software, now it works fine.