cancel
Showing results for 
Search instead for 
Did you mean: 

"Device is not connected" Error in Motor Control Workbench 5.4.6 with X-NUCLEO-IHM07M1 and STM32F302R8

sundar_mepco
Associate

I am attempting to evaluate motor control using the X-NUCLEO-IHM07M1 power board with the STM32F302R8 Nucleo board. I have installed STM32 Motor Control Workbench version 5.4.6 on my PC. However, I encounter the following issue:

Error: "Device is not connected"

Steps Taken:

  1. Hardware Setup:
    • X-NUCLEO-IHM07M1 is stacked on STM32F302R8 board.
    • USB connection is made via STM32’s USB mini port to the PC.
    • Power supply is connected to the motor driver board.
    • Verified jumper settings as per user manual (JP1, JP5, etc.).
  2. Software Checks:
    • USB connection is recognized in Device Manager as STLink (driver is working fine).
    • Attempted connection via Motor Profiler, but it failed to detect the board.
    • Verified that COM port is correctly assigned and visible.
  3. Motor Control Workbench:
    • Attempted to connect in the tool after selecting the correct Nucleo board and firmware version.
    • Tried both "New Project" and “Monitor” mode — same error: “Device is not connected”.
  4. System Info:

    • Windows Version: windows 10
    • STM32CubeIDE: STM32CubeIDE 1.18.1
    • ST-Link Driver Version: 2.2.0
    • Motor Control Workbench Version: 5.4.6
    • X-NUCLEO-IHM07M1 Board
    • STM32F302R8 Nucleo Board
    • Firmware Version: V2J37M26
0 REPLIES 0