2021-04-22 6:05 AM
I have a question about connecting of the SMPS V15SMPS pins. From the datasheet we see, that the V15SMPS_1 and V15SMPS_2 pins are connected internaly. But, on the "Figure 6. SMPS step down converter power supply scheme" they are alco connected externally.
So, the question is: should I externally connect V15SMPS_1 and V15SMPS_2 pins on my PCB or not.
2021-04-22 7:45 AM
Hello
One of the reasons that power pins are multiple is to well distribute flowing currents on silicon chip.
IMO both pins must be connected.
2021-04-23 4:53 AM
Hi Dmytro Medvid,
V15SMPS_1 and V15SMPS_2 pins are already connected internally in the chip.
For the PCB, you should connect these pins externally.
Please refer to the AN5211 for more details (p33/40).
Best Regards,
Ons.