cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4P5G-DK compatibility

Sarvesh_2
Associate

Hello,

 

Is the STM32L4P5G-DK Discovery Kit also compatible with other STM32L4P5xx components, not just the STM32L4P5AG?

 

Thanks in advance,

Sarvesh

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Sarvesh_2 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

The STM32L4P5G-DK is a discovery Board based on the STM32L4P5AGI6P. If you are looking for MCUs pin to pin compatible with the STM32L4P5AGI6P. You can use the pinout compatible option on the STM32CUBEMX:(the picture is not for the L4 bit just an example)

STTwo32_0-1709325282103.png

 

Does this answer your questions.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @Sarvesh_2 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

The STM32L4P5G-DK is a discovery Board based on the STM32L4P5AGI6P. If you are looking for MCUs pin to pin compatible with the STM32L4P5AGI6P. You can use the pinout compatible option on the STM32CUBEMX:(the picture is not for the L4 bit just an example)

STTwo32_0-1709325282103.png

 

Does this answer your questions.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hey STTwo-32,

That's perfect, thanks for the help!

Sarvesh