2021-07-13 05:15 AM
I am in the process of designing a new controller for a product and the only processors that seem available in any quantity are the -P versions. The datasheet isn't clear for these if the SMPS is optional and you can just use the internal LDO, or if you *have* to supply the core voltage separately on these devices.
If we are just losing two I/Os then that's not a problem, if we have to add an external power circuit then it's a different matter.
The datasheet seems to suggest it is the former, but I'd prefer some clarfication on this so I don't design a dud board without realising!
Thanks.
Solved! Go to Solution.
2021-07-13 07:12 AM
You can still use the LDO on this chip, you just lose some pins due to the SMPS capability.
2021-07-13 07:12 AM
You can still use the LDO on this chip, you just lose some pins due to the SMPS capability.
2021-07-13 10:24 AM
Thanks, that's what I was hoping.