2025-02-06 3:30 PM
I have the below code, which is supposed to update DAC with sinewave via SPI3 bus. It was configured and working fine via discrete command, but when I used timer7 to generate an event and update DAC16 via SPI3 via the HAL library, it went to hard fault. I have never seen this before. What caused the hard fault to occur?
I use Nucleo STM32L476 and updated IDE and drivers.
Note I have not included the /CS code (yet) because I was trying to figure out what caused the hard fault. I use optimization -Ofast.
#define DAC16_CENTER (32768)
bool FID_DAC16_Timer7_Sinewave_Event(void)
{
volatile static uint16_t DACSine_Pointer=0;
//--------------------------------------------------
zFID_Obj *zFIDObj = (zFID_Obj *)zFIDHandle; // assign the object (local) utobj->
//--------------------------------------------------
uint16_t dacdata = FID_SineWaveTable[DACSine_Pointer];
if (DACSine_Pointer >= FID_SinewaveSise)
{
DACSine_Pointer= 0;
}
else
{
DACSine_Pointer++;
}
//------------------------------- Process amplitude adjustment while keeping center center.
int32_t centered = (int32_t)dacdata - DAC16_CENTER;
centered = centered / zFIDObj->DACSine_Amp;
dacdata = (uint16_t)(centered + DAC16_CENTER);
//------------------------------- Write data to SPI
uint8_t data[] = { dacdata & 0xFF, dacdata >> 8 }; //flipped for proper ordering of MSD.
HAL_SPI_Transmit(&hspi3, data, 1, HAL_MAX_DELAY); // Hard fault crashed event.
//FID_SPI_WriteData16Simple(FID_CS1_DAC16A,dacdata);
return true;
}
Solved! Go to Solution.
2025-02-06 3:35 PM
2025-02-06 3:35 PM
I forgot to mention I use 16-bit SPI data, but the HAL SPI transmit and received are working fine when not running from Timer7.
2025-02-06 3:35 PM
@Riscy24 wrote:What caused the hard fault to occur?
2025-02-17 5:33 AM
Thank for the link, very useful. It turned out it was divided by zero hard fault. Nothing to do with HAL library which is a relief.
Lesson learnt and moving on!
R.