cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L1 Disco: Can't update ST-Link - unknown firmware version

JohannesM
Associate II

Hello community,

I can't debug my program on my STM32L1 Disco because of the attached message.

JohannesM_1-1730719569809.png

This in itself is not the problem, the problem is that I can't auto-update because it doesn't know what firmware is installed on the board itself!

JohannesM_0-1730719553965.png

What can I do or what am I doing wrong?

I am using the latest CubeIDE (1.16.1).

 

Thanks in advance, you are my last hope.

 

Best regards.

Johannes

 

1 ACCEPTED SOLUTION

Accepted Solutions

What happens if you click 'Open in Update Mode' ?

 

Does STM32CubeProgrammer do the same?

View solution in original post

5 REPLIES 5

What happens if you click 'Open in Update Mode' ?

 

Does STM32CubeProgrammer do the same?

SofLit
ST Employee

Hello,

Disconnect and reconnect your USB cable and try again.

Did you try with ST-LINK firmware upgrade tool?

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

It used to say that the card was not in configuration mode. I reset it and rebooted, but did not unplug it. When I unplugged it, it worked. I did the upgrade, wrote a little test program and it works.

Thank you very much.

It used to say that the card was not in configuration mode. I reset it and rebooted, but did not unplug it. When I unplugged it, it worked. I did the upgrade, wrote a little test program and it works.

Thank you very much.

You're welcome.

Note that everyone can see all posts - there's no need to repeat a post.

You can mention multiple people in a post using