cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7B3 No Display

maununez
Associate II

Hello;

 

I need your support to resolve an issue with the STM32H7B3.

Today once I connected the board to my PC; I noticed that nothing pops up in the display;; I mean... black screen. 

But ... I can see the green lights over the board on and I'm able to connect it thru the SMT32CubeProgrammer

here is an Image:

maununez_0-1689883260955.png

is connected.

 

What can I do to see graphics over the display?

 

Thanks in advance and your support 

 

 

6 REPLIES 6
TDK
Guru

Your screenshot shows that the FLASH is erased (0xFF). That means there is no program on the board, so nothing is sending data to the display.

Is this a STM32H7B3I-DK? You can re-flash the demonstration firmware if you can find it. I can try to look...

If you feel a post has answered your question, please click "Accept as Solution".
TDK
Guru

Redownload the demo firmware here:

https://www.st.com/resource/en/compiled_demos/stm32h7b3i-dk_demo.zip

If you feel a post has answered your question, please click "Accept as Solution".
FBL
ST Employee

Hello @maununez, Welcome to ST Community.

 

Your chip seems to be fully erased. Would you please specify the expected behavior? 

Flashing the demo would be a good start to test the LCD panel.

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


I'm out of offce with limited access to my emails.
Happy New Year!

Thank you TDK | Evangelist for your quick support.

I'm going to follow your instructions .. I mean re-flash the board

I'll share the result

 

Thank you @FBL for your support

As @TDK suggested too

I'll re-flash the board and soon I'll share the result

 

best regards;

Hello Again @TDK 

 

I did the step; the re-flash, but looks like there is a problem once STM32CubeProgrammer try to delete the external memory

maununez_0-1689969594640.png

in the next image; you can see that... I'm trying to upload the demo.hex

 

maununez_2-1689969862120.png

and I have as External loader the one which is in the next image:

maununez_3-1689969963202.png

In resume: the problem is when then CubeProgrammer is trying to delete External Memory

Once again, thank you for your support.

what can I do?

best regards.