2021-07-24 04:03 AM
Hi there,
we are currently designing a sandwich board for the STM32H747i-DISCO board and we want to connect via CN8 and CN5. So far I have only found technical drawings in dm00504240.pfg (see attachment). But the exact position of the two connectors is not specified there.
Any help is highly appreciated!
JSchn.4
2021-07-24 12:08 PM
You can look at the Gerber files if the dimensions given in the user manual are not sufficient. Look in CAD resources for the Board Manufacturing Specifications.
https://www.st.com/en/evaluation-tools/stm32h747i-disco.html#cad-resources
2021-08-17 01:39 AM
@TDK , thanks a lot for your help.
Unfortunately, I am still loosing the needed information. On KiCad, i am not able to open the Gerber Drill files. Get the error message: "Tool 0 not defined".
All I need is the exact position of the CN8 and CN5 and the 4 drill holes for the MB1166.
Would really appreciate your help!
Johannes
2021-08-17 02:47 AM
2021-08-17 03:41 AM
@TDK , thanks again for the quick response.
Unfortunately, I can only assume the exact measures, since gerbv does not have access to the properties of the element. See attached screenshot
2021-08-17 03:46 AM
2021-08-17 03:47 AM
Thanks a lot, I will contact you again in a week!
Johannes
2021-08-27 06:29 AM
@TDK
Did you find the time to look for the specific data?
In addition to the exact position of the connectors, we want to put the LCP display into a case, I would like to know what the radius of the MB1166 display is exactly.
Thanks a lot
Johannes
2021-08-27 12:30 PM
The .ART files are the Gerber files to look at. Looks like you are looking at a dimension file.
To center of mass from left side (x=0) and bottom side (y=0):
CN8: 3.453, 0.743
CN5: 3.193, 2.643
I can't find the datasheet for the LCD. The radius is probably in there.
2021-08-27 01:21 PM
@TDK : Thanks a lot!