cancel
Showing results for 
Search instead for 
Did you mean: 

stm32H743zi pin configuration

Rahu2710
Associate

My hardware has the I2C pins (SDA and SCL) connected incorrectly, and I cannot change them because the hardware is already built. Is there any way I can fix this issue from the firmware side? Can I change the pins through software? hear attach my schematic photo . atck pin are incorrect and i can  not change it. please help me .

 

 

Rahu2710_0-1737701437236.pngRahu2710_1-1737701494796.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief III

>Can I change the pins through software?

no.

You can :

a - take a cutter and wires , cross connect the 2 lines (if this is just one board for proto)

b - make a new board, with correct connection (if thousands of them should be produced)

c - write a software-I2C and use the pins, as they are .

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
AScha.3
Chief III

>Can I change the pins through software?

no.

You can :

a - take a cutter and wires , cross connect the 2 lines (if this is just one board for proto)

b - make a new board, with correct connection (if thousands of them should be produced)

c - write a software-I2C and use the pins, as they are .

If you feel a post has answered your question, please click "Accept as Solution".