cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 Wafer Size

IAhme.3
Associate II

I need to know STM32H7 Wafer Size please

5 REPLIES 5
Imen.D
ST Employee

Hello @IAhme.3​ and welcome to the Community ��

For what purpose?

or do you mean chip size? For that, please have a look at the STM32H7 Datasheet and you will find here the package information and PCB design rules.

Datasheet - STM32H750VB STM32H750ZB STM32H750IB STM32H750XB - 32-bit Arm® Cortex®-M7 480MHz MCUs, 128 Kbyte flash, 1 Mbyte RAM, 46 com. and analog interfaces, crypto

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Probably around 200 or 300 mm depending on the fab.

Or the die size?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Wafer Size/Diameter not chip size​

I think so also, I searched to much but not found certain value​

Crolles is a 300 mm / 12" fab (VQ)

https://www.mouser.com/PCN/STMicroelectronics_8204.pdf

I think TSMC Fab 14 also sources the H7's

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..