2020-01-30 5:37 PM
The logs are below:
17:32:34 : ST-LINK error (DEV_CONNECT_ERR)
17:32:34 : ST-LINK SN : 066CFF545057717867203340
17:32:34 : ST-LINK FW : V2J35M26
17:32:34 : Voltage : 3.21V
17:32:34 : Error: ST-LINK error (DEV_TARGET_CMD_ERR)
I attempted flashing the MCU on the dev kit using command line commands (mbed compile...) and I flashed a blink LED program. Since then, I've not been able to connect to STM32 cube to erase/reprogram the device. How do I recover the dev kit?
Thank you!