2020-12-17 8:54 PM
안녕하세요 .저는 STM32746G-DISCO 보드로 작�?� 프로�?트를 개발하고 있습니다.
STM32746G-DISCO 보드�?
st �?서 제공하는 �?�모 �?�미지 파�?� STM32746G-DISCO_Demo_V1.5.0.hex external loader(N25Q128A_STM32F746G-DISCO) 로 다운로드 하면 아래와 같�?� 0x90000000 번지 programming 할때 �?러가 발�?합니다.
그래서 �?�미지가 나오지 않습니다.
STM32CubeIDE 1.5.0 - TouchGFX 4.15.0 Designer 프로�?트를 만들면 외부 flash n25q_128mb_1_8v_65nm �?� 사용하�?��?�
실제 보드�?는 MT25QL_QLHS_L_128_ABA_0-1287003 외부 flash가 달려 있습니다.
(회로�?� revision 보면 2019년 7월 17�?� 외부 flash가 n25q128 --> MT25QL128 변경 �?�었다고 합니다.)
외부 flash 쓰는 방법�?� 알려 주세요.
Solved! Go to Solution.
2020-12-22 1:45 AM
Even the demo code on the STM32F746G-DISCO board cannot be uploaded. Even if I look at the data sheet, it is in the early stages of development, so I don't know how to write the source code. The demo binary, the initial GUI of the development board, is also not flashed. Can you get help writing the source code?
2020-12-22 12:57 PM
I don't work for any of the parties involved. I can write loaders under contract.
As I remember the details the 25QL128 isn't supposed to support CMD 0x12 but rather (0x38) 0x32 for (EXTENDED) QUAD INPUT FAST PROGRAM
2020-12-23 2:19 AM
I tried using the data sheet you mentioned, but it didn't work, I am going to purchase and test the MT25QL256 and MT25QL512 parts using the MT25QL512 example from the ST external loader making site.
2020-12-23 3:57 PM
한국분 같으신�?� 죄송한�?�요.
누구신지 문�?�드려요.
왜그러�?면 님�?� 쓰진 글�?� 저�?� 계정과 연결�?�어 메�?��?� 옵니다.
2020-12-23 4:01 PM
Dear Imen,
Nevertheless, I change my account nickname of ST Community
I still receive a E-mail from ST Community<community@st.com> about ljeon.1 posts.
Please, check my account.
2020-12-23 4:06 PM
You're probably getting emails now because you were mistakenly tagged into the conversation, not because your accounts are linked.
Try Unfollowing the thread.
2020-12-29 12:21 AM
I am still developing using the STM32F746g-disco board, but the initial screen of the development board GUI does not work properly, and even though I made it using the ST external loader creation site, it does not work properly. If you have a loader made of MT25QL128, which is SD RAM changed from N25Q128A, please share it. The initial screen of the development board is also not working and is not in progress.
2020-12-29 12:22 AM
I am still developing using the STM32F746g-disco board, but the initial screen of the development board GUI does not work properly, and even though I made it using the ST external loader creation site, it does not work properly. If you have a loader made of MT25QL128, which is SD RAM changed from N25Q128A, please share it. The initial screen of the development board is also not working and is not in progress.