cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407-Discovery Reset Delay When Power Applied.

AAhme.41
Associate II

Dear All,

I have a STM32F407-Discovery Kit, I have a problem that when I Power up my Discovery Kit it takes 2 to 3 Seconds to initialize, and during this time there is Garbage values on GPIO Pins. Please tell me what is the problem?

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Karl Yamashita
Principal

If you don't post any code, then we don't know what you're trying to initialize.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Probably the ST-LINK holding it reset.

Check if there is a solder bridge for NRST you can unmake.

Still likely to be a brief delay from your code starting to the point you initialize the clocks/pins. Understand the flow of the code and what it is doing, and where along the time line.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks for your answer, When I connect & power it through USB Cable then it does take any delay, it takes delay only when I Power it from VDD Pins. I Comment all the code just setting the GPIO pins in startup.

I am using new version of STM Cube IDE and using HAL functions

Karl Yamashita
Principal

Sounds like you're not powering up the Discovery board correctly. Have you checked to see when you power VDD that the voltage isn't rising slowly to 3V? Is X2 oscillating right away when you supply power to VDD? Or maybe an issue with NRST pin staying low briefly before going high?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source