cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407-Disc1: UART1 on PA10+PA9 does not work

chkolli
Associate

My company has purchased STM32F407G-Disc 1 board for evaluation in order to use STM32F407VE in our hardware.

UART6 (PC6 + PC7) works fine but UART 1 (PA10 + PA9) does not work.

I found in some old posts that in the discovery board there is a large capacitor connected to PA9 that prevents the uart from working.

Is this true? Does this mean that in my final hardware design there will be no such issue and UART 1 will work fine?

Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
Ozone
Principal

Yes, I remember that much.
The schematics are available on ST's website, check for yourself.

By the way, this is what the user manual has to say about this topic :

Ozone_0-1750062454009.png

Always a recommended read.

View solution in original post

2 REPLIES 2
Ozone
Principal

Yes, I remember that much.
The schematics are available on ST's website, check for yourself.

By the way, this is what the user manual has to say about this topic :

Ozone_0-1750062454009.png

Always a recommended read.

@chkolli also in the User Manual:

AndrewNeil_0-1750063226448.png

https://www.st.com/resource/en/user_manual/um1472-discovery-kit-with-stm32f407vg-mcu-stmicroelectronics.pdf#page=21

via: https://www.st.com/en/evaluation-tools/stm32f4discovery.html#documentation

 

The User Manual tells you that both PA9 and PA10 are occupied by USB:

AndrewNeil_1-1750063429457.png

 


@chkolli wrote:

Does this mean that in my final hardware design there will be no such issue and UART 1 will work fine?


Yes - but you then won't be able to use USB on those pins.

Check the Datasheet to see if there are any other restrictions ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.