2014-09-11 08:26 PM
Used St-link 3.4.0 to read the boards demo program the wrote back, demo does not work anymore, same for 407 and 401 models. do I need to set options different maybe.
#st-link2014-09-12 10:13 AM
No I'd expect you just need to make sure you read out a sufficiently large portion of the flash, and write it back to the same address in an erased device.
2014-09-12 10:25 AM
Attached is a .HEX for the STM32F401C-DISCO
________________ Attachments : 401cdisco.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzoW&d=%2Fa%2F0X0000000bPx%2Fq5SVzIyNyt8lCLfUrl1sKrdkdbwi2tYl7wXFFuaWdOI&asPdf=false2014-09-13 08:59 AM
Hi, Thanks for the file, I guess the full erase was the trick. The file I read the other night was the same length though and does not work. who knows. After working with Pics,Atmels and Tms430's this is a Beast, the GNU tool Chain is a Headache to. But should be fun.
Bill