cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103C8Txxx custom board, glitches after few seconds

MDebo.1
Associate II

Hello everybody,

I made for school a custom stm32f103C8Txxx board.

Programming with a ST-Link V2 work without a problem.

To test the pcb, there are 2 led's (pin pc13 en pa10), they both illuminate every 500ms (easy code to test functionality).

The code wil run, for a few seconds and then glitches and does not respond... even after reset, it will glitch instantly.

If I dissconnect power for a minute, it will work again, but only for a few seconds and then glitches again.

Any ideas what it could be?

I added the schematic for everyone to see (don't mind the usb-c stuff, those components are not place on the pcb)

Edit 1:

Boot 0 and Boot 1 are determined with jumpers. Some parts of the schematic are based on the blue pill.

12 REPLIES 12

my code is made in arduino, converted in bin and then uploaded by STM32 ST-LINK Utility.0693W000005BQr8QAG.png

But I assume pc13 would still work for just blinking a led? it's the same on a blue pill? Didn't really look into that.

The reference manual says PC13-15 should not be used to drive loads like LEDs, but I’ve done so (before I knew better) and never had issues. YMMV.
If you feel a post has answered your question, please click "Accept as Solution".