2019-11-25 06:47 AM
issue-when programming using the Command line utility it indicates success but the unit does not boot. when programming from the GUI the unit powers up correctly. I used the same command line on an st32f07 without issue. Here is the command line. start /B/wait st-link_cli.exe -c SWD UR -ME -P c:\RF6_RP_FAC_1.5.bin 0x8000000. Am I missing a setting/command? I attached a screen shot of the firmware in the stlink programming utility