2024-06-03 1:46 AM
Hi,
I am looking for a SD Card image from STM32F072B-EVAL kit. Without it demo program can not run. Package from ST site (en.stsw-stm32137) contains files from SD card, but it seems it does not work. I will be grateful for help.
2024-06-03 4:15 AM
Welcome @pawelr, to the community!
the STM32072B-EVAL is obsolete, but the firmware is still available. The STSW-STM32137 not only contains the media data for the SD card, but also the firmware for the STM32F072VBT6 in a file called stm32072B-eval_fw_v1.0.0.hex.
Hope that helps?
Regards
/Peter