cancel
Showing results for 
Search instead for 
Did you mean: 

STLINK-V3PWR VCP not working

VK Verma
Senior

Hi,

I tried it on two different STLINK-V3PWR tools and its VCP(RX and TX) is not working after shorting the RX and TX pin with external jumper to bring it into loop back test.

Is there any remedy for this ?

Regards,

VK Verma

 

2 REPLIES 2
AScha.3
Chief III

i made test: V3mods , pin 12 -> pin15 ; tx-rx ; start arduino2 -> ser.monitor ; write: hello loopi

no problem:

AScha3_0-1689417743710.png

should be same on your V3pwr vcp port

If you feel a post has answered your question, please click "Accept as Solution".
MS75
ST Employee

Hello @VK Verma ,

For your test do you first supply the BRIDGE's TVCC pin with the target voltage? (more details on chapter 7.4.1 page 15 of the UM3097 STLINK-V3PWR)