cancel
Showing results for 
Search instead for 
Did you mean: 

STLINK-V3MINIE and bluePill

Blueicaro
Associate

Hello, I new with embedded hardware. I have a bluepill (original) and STLINK-V2 debugger (a not original).

And now, I want to change the my STLINK-V2 for a new one, which I can make debug, not only programming.

I found the STLINK-V3MINIE. But I'm sure if can be used with bluepill, any one used this debugger with bluepill?. Any issue using it?.

Thanks in advance

/BlueIcaro

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Blueicaro and welcome to the ST Community :smiling_face_with_smiling_eyes:.

If you are using original MCUs, it should work without issue since the STLINK-V3MINIE is designed to support All STM32 MCUs.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @Blueicaro and welcome to the ST Community :smiling_face_with_smiling_eyes:.

If you are using original MCUs, it should work without issue since the STLINK-V3MINIE is designed to support All STM32 MCUs.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.