2022-04-25 7:47 AM
After this second trial, the only way that I'm able to program the MCU is using the JLINK, but I would really need the STLINK-V3MINI working as expect.
2022-04-25 8:16 AM
Hello @RBitt.1
Are you able to test is with a STLINK V2 ? Can you give me the version of STMCubeProgrammer you are using ( STM32_Programmer_CLI.exe -version) ?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-04-25 9:02 AM
Hi Bruno,
tested with STLINKv2 -> same issue
Cube updated to 2.10.0, tested with 2.9 as well, same issue.
2022-05-02 3:59 AM
Hi Bruno,
Is there any news/suggestion to test?
Thank you!
2022-05-02 3:28 PM
As always - use "connect under reset" and "hardware reset" modes.
2022-05-02 11:51 PM
Ciao @RBitt.1
Sorry about the delay, it took me some time to find a STMF board.
I confirm that the right way to program is to execute the following command :
STM32_Programmer_CLI.exe -c port=SWD mode=UR -d <file_to_program> -ob rdp=0xBB
That should download the file and lock the device in RDP level 1. If you want to verify the download just, add -v just before -ob.
To unlock the part, (mass erase will be performed automatically), execute
STM32_Programmer_CLI.exe -c port=SWD mode=UR -ob rdp=0xAA
Is it ok for you ?
BR,
Bruno
PS: Please select as best answer to improve best hit on query
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.