Skip to main content
ABric.2
Associate II
September 7, 2022
Question

STLink V3 Mini couldn't connect to target sometimes

  • September 7, 2022
  • 0 replies
  • 564 views

Hi

I'm using STLink-V3 Mini probe to flash and read UID of a stm32F401RET6 with STM32Cubeprogrammer command line under ubuntu 2022.

Here is the command I'm using : "<path to STM32_Programmer_CLI -log <log_filename> -c port=SWD mode=UR freq=4000 -rdu -r32 0x1FFF7A10 0x10"

(I try with different mode (Normal, UR,...) but it didn't change)

Most of the time it works well, but sometimes, it return the error : "No STM32 target found!"

All the connections are corrects as the read ID test pass most of the time.

When it fails, it's fail for few test in a row, I'm forced to change device, read the UID, and go back to the first one. This error happens with multiple device.

Any idea of why it can fails ?

Thanks in advance,

Antoine

This topic has been closed for replies.