2025-08-17 11:33 PM
Can X-NUCLEO-IHM09M2 (adapter board) connect with NUCLEO-H755ZI-Q (controller board) using male and female connector(without flying wire)?
Solved! Go to Solution.
2025-08-18 7:27 AM
Hello @Maverick,
You must verify that all the required signals are available. If they are not available, add the necessary wires and update the X-NUCLEO-IHM09M2.json file located in the MC_SDK_x.x.x\Utilities\PC_Software\STMCWB\assets\hardware\board\adapter directory.
2025-08-18 7:27 AM
Hello @Maverick,
You must verify that all the required signals are available. If they are not available, add the necessary wires and update the X-NUCLEO-IHM09M2.json file located in the MC_SDK_x.x.x\Utilities\PC_Software\STMCWB\assets\hardware\board\adapter directory.