2016-08-16 08:32 AM
Hello, I have trouble setting a STLink, been looking alone for days but still have no solution. The sensitive points in my opinion will be underlined.
I have a hard time posting photos here because of the max file size.I am using a STLink sawn-off from a Nucleo-L053R8 board, MB1136 revC.I want to access a STM32F427 custom board.The STLink and custom board both boot and are recognized in Windows device manager as STLink debug/STLink virtual COM port and serial USB respectively.When both boards are powered via USB, trying to connect in STLink utility issues a pop-up ''No STLink detected''.The wiring used is SWCLK, GND and SWDIO.
(I assumed that the closest pin to the CN12 jumper, on the CN4 connector, was the 3.3V target.)
I removed CN2 jumpers.I installed ST-Link/V2 v3.9.0 and since repaired it.It installed drivers. Trying to get a connection,afterward I replaced drivers with ones from Zadig,
I then removed drivers from the device manager, and reinstalled the drivers from STSW-LINK009amd64.exe.
I still have not managed to connect with st link utility once, even when I try to connect back to the nucleo chip as described in UM1724...As I understood that Clive1 does a huge job helping others, I will thank him a lot, or anyone that would chime in, for their time spent helping here.Maxime #stlink
2016-08-16 10:33 AM
Problem resolved... ''Ccleaned'' registry. :O