2023-02-20 02:45 AM
A web search tells me I have a problem! My STM32 target has a MIPI10 connection for SWD debugging which works great with my I-jet probe. I now need to use an STLink but none of the supplied cables are for a MIPI10 target. Where can I buy such a cable (or do I really need to make my own adapter)?
2023-02-20 03:04 AM
STLinkV3 is considered a refresh of v2 and has MIPI14 connector as it includes USB to UART translation. You can cut corner pins to get MIPI 10, or you may find JTAG 20 to MIPI adapters online or at ST partner debug probe accessoriee.
2023-02-20 05:02 AM
Isn't that still all 0.1 inch pitch?
2023-02-20 05:27 AM
Aren't there some 10 pin cables with 14 pin header crimped on one end?
2023-02-20 06:00 AM