2013-06-28 5:41 AM
I'm not having any luck getting Windows 8 to load the ST Link driver correctly. Other people have posted similar problems but have reported that setting Windows 8 to disable Driver Signature Enforcement fixes their problems. This hasn't worked for me.
I'm using the ST-Link part of an STM32F4 discovery board to program my own STM32F4 based board. It's worked for me for over a year using Windows 7 on my previous laptop which died last week. I'm rebuilding my development environment on a new Windows 8 laptop (Dell Inspiron 15z) and getting the driver to work is frustrating me. I'm installing st-link_v2_usbdriver downloaded from http://www.st.com/web/en/catalog/tools/PF258167 As an aside, my target board uses USB as a VCP and I've installed the USB VCP driver ok. Does being 64-bit make any difference? I've been into the registry and found the entry for the ST-Link in the enum\USB section. This is what it looks like .. it might mean something to somebody. [HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Enum\USB\VID_0483&PID_3748] [HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Enum\USB\VID_0483&PID_3748\5&2842f95&0&2] ''DeviceDesc''=''STM32 STLink'' ''LocationInformation''=''Port_&sharp0002.Hub_&sharp0003'' ''Capabilities''=dword:00000004 ''ContainerID''=''{27e98665-dfdd-11e2-be75-6817291a1417}'' ''HardwareID''=hex(7):55,00,53,00,42,00,5c,00,56,00,49,00,44,00,5f,00,30,00,34,\ 00,38,00,33,00,26,00,50,00,49,00,44,00,5f,00,33,00,37,00,34,00,38,00,26,00,\ 52,00,45,00,56,00,5f,00,30,00,31,00,30,00,30,00,00,00,55,00,53,00,42,00,5c,\ 00,56,00,49,00,44,00,5f,00,30,00,34,00,38,00,33,00,26,00,50,00,49,00,44,00,\ 5f,00,33,00,37,00,34,00,38,00,00,00,00,00 ''CompatibleIDs''=hex(7):55,00,53,00,42,00,5c,00,43,00,6c,00,61,00,73,00,73,00,\ 5f,00,46,00,46,00,26,00,53,00,75,00,62,00,43,00,6c,00,61,00,73,00,73,00,5f,\ 00,46,00,46,00,26,00,50,00,72,00,6f,00,74,00,5f,00,46,00,46,00,00,00,55,00,\ 53,00,42,00,5c,00,43,00,6c,00,61,00,73,00,73,00,5f,00,46,00,46,00,26,00,53,\ 00,75,00,62,00,43,00,6c,00,61,00,73,00,73,00,5f,00,46,00,46,00,00,00,55,00,\ 53,00,42,00,5c,00,43,00,6c,00,61,00,73,00,73,00,5f,00,46,00,46,00,00,00,00,\ 00 ''ConfigFlags''=dword:00000040 #stm32driver-usb #stlink-driver-not-working2013-06-28 6:27 AM
Aren't ALL x86 Windows 8 64-bit, I guess it's not a
http://windows.microsoft.com/en-us/windows-8/system-requirements
, but I've never encountered a retail PC shipping with 32-bit? The one I was using certainly was 64-bit. What does Device Manager indicate about the ST-Link driver state?2013-06-28 7:33 AM
When I plug in my Discovery Board an ''STM32 STLink'' appears in Device Manager under ''Other devices''
The icon next to it has an exclamation mark on a yellow background. If I bring up the properties window I get .. General ======= Device type - Other devices Manufacturer - Unknown Location - Port_#0004.Hub_#0003 Driver ====== Driver Provider - Unknown Driver date - Not available Driver Version - Not available Digital Signer - Not digitally signed Details ======= ConfigFlags - 00000040 CONFIGFLAG_FAILEDINSTALL amongst many other properties. I've had a rummage in \Windows\Inf and found stlink_winusb.inf It has DriverVer=07/28/2010 in the [Version] section at the top. This file also refers to WdfCoInstaller01009.dll and WinUSBCoInstaller2.dll in %WinDir%/System32. I've found these and they have the following details.. WdfCoInstaller01009.dll File version - 1.9.7600.16385 Size - 1.64 MB Date modified - 14/07/2009 14:21 WinUSBCoInstaller2.dll File version - 6.1.7600.16385 Size - 979KB Date modified - 14/07/2009 07:372013-06-28 9:07 AM
I have a Win 8 64 bit VM and I HAD to use the unsigned driver reboot trick to get the ST-Link driver installed.
But it did install and it works on Win 8 64bit. Don't remember what magic it took to get it installed, it was some time ago and my brain is getting to be more like a FIFO2013-06-28 12:20 PM
I've just done this again on two different PCs, using the ST-Link_V2_USBdriver.exe from \Keil\ARM\STLink\USBdriver
http://i.imgur.com/AHLAjNn.png
http://i.imgur.com/IvlslDD.png
If you had previously installed the driver you want to Update, let the machine find it, and then agree to install when the red hazard warning comes up.2013-06-29 1:41 AM
i had this problem before in my 64 bits windows 7 , so i desinstalled the stm driver and i after that i removed the usb and i installed the usb driver (u can find it in KEIL repository) and then i connected my stm to pc and i updated using st-linkupdate
search in this path C:\xxxxx\Keil\ARM\STLink2013-07-01 3:41 AM
2013-07-18 6:39 PM
Hi I have the same problem but Clive's solution didn't fix it.
I'm also using Windows 8, 64 bit laptop. When I searched for driver update online in the device manager, it shows that:Windows found driver software for your device (STMicroelectronics STLink dongle) but encountered an error while attempting to install it.Does anyone have the same problem? How shall I solve it? I got stock here for a day...Thanks a lot!!2013-07-18 6:54 PM
I found the solution somewhere in the threads. Thanks to Clive for your previous post!
unsigned and signed device is really annoying... :(2013-07-18 7:06 PM
I posted a link to it earlier in the thread, and I think Ian had already tried that technique, but after he had installed the driver.
/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/ST-LINK%20under%20Windows%208&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=192
I found the following page useful to permit the installation of the unsigned ST-LINK driver under Windows 8
http://www.trickday.com/2012/09/how-to-install-unsigned-drivers-in-windows-8/