cancel
Showing results for 
Search instead for 
Did you mean: 

St-Link V3 SWD to stm32L452 JUST DOES NOT WORK

SLevi.1
Senior

Cube programmer (and st-link utility) cannot find the target when I try to connect to flash a device. I am using the SWD connection to my target. I have connected T_Vcc, gnd, clk, dio & nrst on CN6 of the MB1440B mezzanine board. Cube programmer recognises the st-link, sees 3.2v on the target vcc, but always reports "Error No STM32 target found".

I have tried the same connections on the same target using a st-link V2 on a Nucleo board, and that works ok. I have also tried the Nucleo against a blue pill target, and again that works. Neither target is recognised by the st-link V3. Are there any special settings in cube programmer (or st-link utility) I need to look at? As far as I know, I have the latest drivers and firmware installed on the st-link v3.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Aziz BRIGUI
ST Employee

Hello @nonesuchevitt​,

Thank you for posting and sorry for the late reply,

I couldn't reproduce your issue on my side, could you please describe your connections precisely. I tested using a NUCLEO-L452RE, my connections are as follows (Please refer to UM1724 page 28) :

STLINK-V3 (CN6) | NUCLEO-L452RE

T_VCC => CN6 (4)

CLK => CN7(15)

GND => CN6(6)

DIO => CN7(13)

NRST => CN6(3)

I was able to connect using STM32CubeProgrammer and ST-LINK Utility. As far as I know, there are no special settings to configure.

Looking forward to your response.

Best regards,

Aziz


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SLevi.1
Senior

Thanks for taking the time to answer. However, it still does not work. I connected a Nucleo452RE board as you specified, and powered it via the nucleo USB mini port. I removed the CN2 jumpers at the top of the nucleo board just in case. In the STM cube programmer output I see only:

 17:24:10 : ST-LINK SN : 001900283137510839383538

 17:24:10 : ST-LINK FW : V3J9M3B5S1

 17:24:10 : Board    : STLINK-V3SET

 17:24:10 : Voltage   : 3.26V

 17:24:10 : No STM32 target found!

 17:24:10 : ST-LINK SN : 001900283137510839383538

 17:24:10 : ST-LINK FW : V3J9M3B5S1

 17:24:10 : Board    : STLINK-V3SET

 17:24:10 : Voltage   : 3.26V

 17:24:10 : Error: No STM32 target found!

Does seem a bit odd, have you tried knocking down the connection speed to 1 or 2 MHz?

Or connect/reset options. Behave differently with BOOT0 pulled HIGH?

Device's tend to go into low power modes

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
SLevi.1
Senior

I've tried all different combinations of connection speed, frequency, reset mode etc. Still no joy.