2019-01-31 1:47 PM
I installed the driver for the ST-LINK V2 on Windows 10 (STSW-LINK009). The Installation was successful. Unfortunatelly the device can't connect to the USB port and is blinking red. I even can't find the driver in the Device Manager in Windows. The software tools from st can't also find any device. I've tried it on three computers, with the same result.
Solved! Go to Solution.
2023-11-14 1:06 AM
try stm32CubeProgrammer - this should work.
2023-11-14 2:39 AM
I have stm32CubeIDE already installed. Can I use that to program my board with a .bin file? If yes. How?
2023-11-14 3:02 AM
to load just a bin -> stm32CubeProgrammer is the tool to use.
2023-11-15 7:54 AM
My problems with the dongle have now been resolved. In the hope that this may help somebody else this is what I did.
Since the dongle was working properly on a different computer I inserted a USB externally powered hub between the dongle and the computer. This fixed the issue for me so I think the problem was a signal level issue.
Also I did not need to install the Cube Programmer (thanks anyway AScha.3) to fix the STSW programmer issue. For some reason the zip file for STSW-LINK009 did not contain the setup.exe program when extracted. Only the drivers. Since I still had the old folder STSW-LINK004 I ran setup.exe from this folder and the STSW programmer got reinstalled again. When I checked the drivers via Device Manager, the system confirmed that I had the latest.
2024-04-15 10:59 AM
Thanks, your tip saved me
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.