cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link - Failed to stop the target

Rogers.Gary
Senior II
Posted on March 26, 2015 at 06:25

Hi,

I'm using IAR EWARM 7.3. I'm using ST-Link, newest firmware. The target is connected via JTAG. It flashes and seems to run OK - the IWDG is ticking fine without crashing, with RTOS running. I can print using ITM_Sendchar(). The Debugger option is set for ''Connect during reset''

After launching the application, there are 2 odd things happening. First, when I try to stop the application (Red X) I get the pop-up dialogue that says ''Target is running, Failed to stop the target''

The other is the SWO trace output. Each time I run the debugger, it does not ''save'' the trace output settings I have to keep checking the boxes for ITM0 output.

Any suggestions? I could not find anything in the forums...

Thanks.

#stm32f4 #st-link
0 REPLIES 0