2024-07-16 12:04 AM
HI, STM Experts,
Using STM32CubeIDE, I configured a project with default settings for the STM32H563ZIT6 (8 MHz external clock), running at 250 MHz. Additionally, I've enabled SPI1 for full duplex communication (transmitting and receiving simultaneously), with a data size of 8 bits, clock polarity (clk pol) = 0, clock phase (clk ph) = 1, and set the prescaler to 2, resulting in a baud rate of 125.0 Mbits/s. It's usually possible to wire MOSI to MISO. However, when I try to receive data from SPI1, it doesn't work. I don't know where I made a mistake. Could anyone please support me?
uint8_t tx_buffer[] = { 'H', 'e', 'l', 'l', 'o', '\r', '\n' };
uint8_t rx_buffer[20];
while (1)
{
//HAL_UART_Transmit(&huart7, tx_buffer, sizeof(tx_buffer), 100);
HAL_Delay(1000);
for (int i = 0; i < sizeof(tx_buffer); i++)
{
HAL_SPI_TransmitReceive(&hspi1, tx_buffer + i, rx_buffer, 1, 100);
HAL_UART_Transmit(&huart7, rx_buffer, sizeof(rx_buffer), 100);
HAL_Delay(200);
}
}
static void MX_SPI1_Init(void)
{
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 0x7;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
hspi1.Init.ReadyMasterManagement = SPI_RDY_MASTER_MANAGEMENT_INTERNALLY;
hspi1.Init.ReadyPolarity = SPI_RDY_POLARITY_HIGH;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
}
2024-07-18 4:54 AM
Can you show us what you do?
2024-07-18 5:53 AM
#include "main.h"
#include "string.h"
#include "stdbool.h"
SPI_HandleTypeDef hspi1;
SPI_HandleTypeDef hspi2;
UART_HandleTypeDef huart7;
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ICACHE_Init(void);
static void MX_SPI1_Init(void);
static void MX_UART7_Init(void);
static void MX_SPI2_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
uint8_t tx_buffer[] = "Hitman Sharma\r\n";
uint8_t rx_buffer[20];
bool rx_complete = false;
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
HAL_Init();
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ICACHE_Init();
MX_UART7_Init();
MX_SPI1_Init();
MX_SPI2_Init();
while (1)
{
HAL_Delay(1000);
HAL_SPI_Receive_IT(&hspi1, rx_buffer, sizeof(rx_buffer));
HAL_SPI_Transmit(&hspi1, tx_buffer, sizeof(tx_buffer), 100);
HAL_Delay(200);
if(rx_complete == true)
{
HAL_UART_Transmit(&huart7, rx_buffer, sizeof(rx_buffer), 100);
}
}
}
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
if(hspi->Instance == SPI1)
{
rx_complete = true;
}
}
static void MX_SPI1_Init(void)
{
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 0x7;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
hspi1.Init.ReadyMasterManagement = SPI_RDY_MASTER_MANAGEMENT_INTERNALLY;
hspi1.Init.ReadyPolarity = SPI_RDY_POLARITY_HIGH;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}
2024-07-18 6:40 AM
You're sending 16 bytes, and waiting until 20 are received. Can you see why this is not working?
2024-07-21 9:52 PM
sorry for my late reply
uint8_t tx_buffer[] = "Hitman Sharma\r\n";
uint8_t rx_buffer[16];
bool rx_complete = false;
i changed its not working
2024-08-05 2:14 AM
Try uint8_t rx_buffer[15];