SPI Loopback test on stm32h563zit6
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-16 12:04 AM
HI, STM Experts,
Using STM32CubeIDE, I configured a project with default settings for the STM32H563ZIT6 (8 MHz external clock), running at 250 MHz. Additionally, I've enabled SPI1 for full duplex communication (transmitting and receiving simultaneously), with a data size of 8 bits, clock polarity (clk pol) = 0, clock phase (clk ph) = 1, and set the prescaler to 2, resulting in a baud rate of 125.0 Mbits/s. It's usually possible to wire MOSI to MISO. However, when I try to receive data from SPI1, it doesn't work. I don't know where I made a mistake. Could anyone please support me?
uint8_t tx_buffer[] = { 'H', 'e', 'l', 'l', 'o', '\r', '\n' };
uint8_t rx_buffer[20];
while (1)
{
//HAL_UART_Transmit(&huart7, tx_buffer, sizeof(tx_buffer), 100);
HAL_Delay(1000);
for (int i = 0; i < sizeof(tx_buffer); i++)
{
HAL_SPI_TransmitReceive(&hspi1, tx_buffer + i, rx_buffer, 1, 100);
HAL_UART_Transmit(&huart7, rx_buffer, sizeof(rx_buffer), 100);
HAL_Delay(200);
}
}
static void MX_SPI1_Init(void)
{
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 0x7;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
hspi1.Init.ReadyMasterManagement = SPI_RDY_MASTER_MANAGEMENT_INTERNALLY;
hspi1.Init.ReadyPolarity = SPI_RDY_POLARITY_HIGH;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
}
- Labels:
-
STM32H5 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-16 1:27 AM
sorry for my post its working good but i have an doubt
i am testing loop back test on spi1 on stm32h563zit6 microcontroller
hardware connection:
spi1:
mosi---------->miso
Whenever I use the HAL_SPI_TransmitReceive function, it works well. However, when I try to use HAL_SPI_Transmit and HAL_SPI_Receive functions instead of HAL_SPI_TransmitReceive , it doesn't work. What could be the problem? How can I make it work?
while (1)
{
HAL_Delay(1000);
HAL_SPI_Transmit(&hspi1, tx_buffer, sizeof(tx_buffer), 100);
HAL_SPI_Receive(&hspi1, rx_buffer, sizeof(rx_buffer), 100);
HAL_UART_Transmit(&huart7, rx_buffer, sizeof(rx_buffer), 100);
HAL_Delay(200);
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-16 1:54 AM
Hello,
When you're calling HAL_SPI_Transmit(), the chip is not ready to receive anything, so it is transmitting in the void.
and when you're calling HAL_SPI_Receive(), nobody is sending anything, so time out occurs.
So, maybe call HAL_SPI_Receive_IT (and prepare the SPI ISR) before transmitting so the chip is ready to receive the data.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-16 2:47 AM
thank you @Mike_ST any reference?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-16 5:04 AM
Related/duplicate:
Solved: SPI LOOP BACK TEST on STM32H563ZIT6 - STMicroelectronics Community
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-16 7:32 AM
@Mike_ST any reference code?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-16 8:18 AM
I mean... people already gave you almost everything above.
As discussed in the topic shared by @TDK, the solution is the same.
Modify your CubeMX project to enable SPI interrupts.
Then run something like this:
bool rx_compltet = false;
int main(void)
{
uint8_t tx_buffer[] = { 'H', 'e', 'l', 'l', 'o', '\r', '\n' };
uint8_t rx_buffer[20];
while (1)
{
HAL_Delay(1000);
HAL_SPI_Receive_IT(&hspi1, rx_buffer, sizeof(rx_buffer), 100);
HAL_SPI_Transmit(&hspi1, tx_buffer, sizeof(tx_buffer), 100);
HAL_Delay(200);
if(rx_complete == true)
{
HAL_UART_Transmit(&huart7, rx_buffer, sizeof(rx_buffer), 100);
}
}
}
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
if(hspi->Instance == SPI1)
{
rx_complete = true;
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-16 10:12 PM
OK.. Thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-17 3:20 AM
Did that helped?
Did you succeed with your loop back ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-18 1:50 AM
No! @SMarie