cancel
Showing results for 
Search instead for 
Did you mean: 

SD-Card function BSP_SD_IsDetected backwards?

Guido Körber
Associate III

It looks like the BSP_SD_IsDetected function from the sample codes is working backwards.

 

According to the SD-Card spec this pin has a weak pullup (50 kΩ) inside the card. So the STM32 should have a weaker pull down on the pin and detect the presence of the card if there is a high on the pin.

But the sample code activates the pull up and checks for a low as the indicator of the SD-Card presence.

5 REPLIES 5
AScha.3
Chief

>SD-Card spec this pin has a weak pullup (50 kΩ) inside the card

Source please ?

afaik

Micro SD-cards - we talk about - right ?

Here the card holder usually has a switch to case/gnd, so its easy to detect a card-is-in , ie with a pin+pullup connected to this switch. Other way is just send command -- and wait for response, or not.

Cd is this card-detect pin:

AScha3_0-1708373384712.png

AScha3_0-1708375979331.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Source: Simplified Physical Layer Specification

https://www.sdcard.org/downloads/pls/pdf/?p=Part1_Physical_Layer_Simplified_Specification_Ver9.10.jpg&f=Part1PhysicalLayerSimplifiedSpecificationVer9.10Fin_20231201.pdf&e=EN_SS9_1

 

That is pin 1 on SD/miniSD and Pin 2 on micro.

 

While the other options may wirk too, detecting the card presence via the CD/Dat3 pin is what the sample code does.

Most sockets have a mechanical switch which grounds when a card is in the socket. It's rather rare for one to use the pull-up in the card itself, as again most sockets for SDIO/SDMMC need pull-ups for signal integrity with pins changing direction in 4-bit modes, and not using 1-bit modes beyond initialization.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Guido Körber
Associate III

Please, this question is about the sample code, not about the SD-Card specs or various sockets.

So again: The sample code for the F7 series seems to do the card detection wrong. I wonder if this has ever been tested?

Here is the function:

uint8_t BSP_SD_IsDetected(void)

{

__IO uint8_t status = SD_PRESENT;

 

/* Check SD card detect pin */

if (HAL_GPIO_ReadPin(SD_DETECT_GPIO_PORT, SD_DETECT_PIN) == GPIO_PIN_SET)

{

status = SD_NOT_PRESENT;

}

 

return status;

}

 

So it definitely decides that the card is not present when the CD-pin is high. In the definitions the D3/CD pin is defined as the SD_DETECT_PIN and the internal pullup of the microcontroller is activated. This definitely can never work.

Use this button to properly post source code:

AndrewNeil_0-1708425709012.png