2021-01-13 7:03 AM
Once I connect st-link v2-1 to STM32G473VBT6, there is a disk added into my PC, and there are 2 files in the disk. One is DETAILS.TXT(Version: V2J37M26 Build: May 13 2020 17:07:43), another is FAIL.TXT (The interface firmware FAILED to reset/halt the target MCU).
If I try to debug in STM32CubeIDE, it shows
"Target unknown error 32
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target."
I tryied to tie Boot0 to high or low, but it did not resolved the problem.
2024-05-24 6:02 PM
No H745ZI-Q , voltou ao normal ao carregar o codico com o botão de reset e usuários acionados ao mesmo tempo
2024-09-23 7:22 AM - edited 2024-09-23 7:23 AM
After my experiments with Flash, I got an identical problem. How I fixed it is, see screen
2025-02-07 5:45 PM
I had this same problem on the STM32H735G-DK and reason of this was a wrong firmware uploaded which blocked SWDIO. All the time ST-LINK-V3E put file named "FAIL.TXT" in the mass storage device entries.
Solution:
Change BOOT switch (showed on the picture below) to SYS MEM possition, plug ST-LINK to USB (now on MSC device doesn't exist "FAIL.TXT" file), run STM32CubeProgrammer and do full erase of MCU flash. Now change BOOT switch to FLASH mark and everything is all right after reset.