2021-01-13 07:03 AM
Once I connect st-link v2-1 to STM32G473VBT6, there is a disk added into my PC, and there are 2 files in the disk. One is DETAILS.TXT(Version: V2J37M26 Build: May 13 2020 17:07:43), another is FAIL.TXT (The interface firmware FAILED to reset/halt the target MCU).
If I try to debug in STM32CubeIDE, it shows
"Target unknown error 32
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target."
I tryied to tie Boot0 to high or low, but it did not resolved the problem.
2024-05-24 06:02 PM
No H745ZI-Q , voltou ao normal ao carregar o codico com o botão de reset e usuários acionados ao mesmo tempo