2024-06-18 02:33 AM - last edited on 2024-06-18 03:09 AM by SofLit
Hello Support Team,
I am trying to use a power bank to supply power to my STM32H743ZI2 board. I have made a modification to the jumper settings: I changed the connection of JP2 from pins 1-2 to pins 7-8 as suggested for power bank usage. However, I am encountering an issue where the LD4 LED is blinking intermittently.
Could you please provide guidance on the following points:
Your assistance in resolving this issue would be greatly appreciated.
Thank you for your support.
Best regards,
Wolf Sripe
Additional Information:
Thank you for addressing this matter at your earliest convenience.
Solved! Go to Solution.
2024-06-18 03:10 AM - edited 2024-06-18 03:15 AM
Hello and welcome to the community.
STM32H743ZI2 is a microcontroller not a board, do you mean NUCLEO-H743ZI?
If yes, the recommendation on how to power the board is provided in the board's user manual (UM2407 or UM2408 following the board you are using MB1363 or MB1364) especially the section "External power supply input 5V_EXT (5 V, 500 mA max)"
2024-06-18 03:10 AM - edited 2024-06-18 03:15 AM
Hello and welcome to the community.
STM32H743ZI2 is a microcontroller not a board, do you mean NUCLEO-H743ZI?
If yes, the recommendation on how to power the board is provided in the board's user manual (UM2407 or UM2408 following the board you are using MB1363 or MB1364) especially the section "External power supply input 5V_EXT (5 V, 500 mA max)"
2024-06-18 07:21 AM
So i cant use with cable usb?