cancel
Showing results for 
Search instead for 
Did you mean: 

Pin 1 and 2 on STDC14 of STLINK-V3SET

BWate.1
Associate

Is it ok to connect boot0 from STM32 (with a 10k pulldown to GND) to one of pin 1 or 2 on STDC14 from STLINK-V3SET?

The pins are 'reserved' regarding to the STLINK-V3SET manual p. 23 with the comment 'Do not connect on target' ;)

The boot0 should be ignored in this case, but we need boot0 for an alternative device.

Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions
Uwe Bonnes
Principal III

Actually PA7 is the SWD direction signal. PA7 high means SWD write, low means read.

View solution in original post

4 REPLIES 4
Uwe Bonnes
Principal III

I checked on a V3 MOD board. There are internal connections on Pin 1/2 and, not like the for the other STDC14 pins, (obvious) 0-Ohm jumpers to isolate. So I would take the advice serious.

Uwe Bonnes
Principal III

https://github.com/RadioOperator/CMSIS-DAP_for_STLINK-V3MINI/blob/master/STLINK-V3MINI/Adaptor/STLINK-V3MINI_GPIOs_v4.JPG

labels STDC14 Pin 1 as PB0, 3.3V output and Pin 2 as PA7. Info at your own risk!

BWate.1
Associate

Thank you for the information.

Yes, I also think to connect something else isn't good...

BTW: Without a connection I have measured on the STDC14 from the STLINK-V3SET:

Pin 1: 5 V

Pin 2: 3,3 V

Uwe Bonnes
Principal III

Actually PA7 is the SWD direction signal. PA7 high means SWD write, low means read.