cancel
Showing results for 
Search instead for 
Did you mean: 

PCB Boards for STM32F429 176 pin or 208 pin versions?

gbarbour
Associate III
Posted on April 30, 2014 at 23:56

.ExternalClassC45DEEA78D324C0E97A656CD9497960D P {margin-bottom:0.08in;} .ExternalClassC45DEEA78D324C0E97A656CD9497960D A:link {;}

Hello,

I would like to design a product based on the STM32F429 chip. I first thought I could do it with the Disco board but there are not enough free I/Os for me to use that unless I use some of the I/Os to drive serial bus expander chips.

I would like to know if anyone knows of any boards, or board designs, that use the 176 or 208 pin versions of this great little MCU?

Scmartboard has an adapter board that might work. (

http://www.schmartboard.com/index.asp?page=products_qfp&id=116

)

But I am wondering if there is anything else available that would let me use the larger versions of this chip without designing my own board for it.

Thank you.

#stm32f429 #discovery #pcb
13 REPLIES 13
belamy
Associate
Posted on December 04, 2015 at 19:30

Hi Tede,

I'm looking for Altium project with STM32F429 and yous idea is very interested. Could I use your solution as base for my?

Could you share your project?

Mark Edwards
Associate II
Mark Edwards
Associate II
Posted on December 06, 2015 at 21:31

Test

Link to STM32F429/Altera CycloneIII & STM32F429 CAN Test Bd's

https://drive.google.com/folderview?id=0BxRVLTyjEy66Q3VPcUxaeE13V28&usp=sharing

0690X00000605K0QAI.png

Self.Glenn
Associate III
Posted on December 07, 2015 at 03:02

Sorry, new to forum, try again:

I have been using these F4 boards for several years. They seem pretty good and can have up to 8MB of PSRAM on-board.

Have only had one breakdown on a heavily used board, probably my fault.

http://www.hotmcu.com/hystm32f4xxcore144-coredev-board-p-10.html?cPath=1_20

Excellent forum and informative posts. Been lurking for a while.

Thanks all...

Glenn