cancel
Showing results for 
Search instead for 
Did you mean: 

On a STM32L4R9 one of our designs wants the VSSSDI pin to be connected to ground through a capacitor (not directly connected to ground) when the DSI is not used. But in the datasheet it states that if DSI is not used it should be grounded?

DAndr.6
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Sarra.S
ST Employee

Hello @DAndr.6​,

Your question is not really clear, what designs are we talking about ?

but the Ref man clearly states :

0693W00000Y8fzlQAB.pngHope that helps!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

DAndr.6
Associate II

Hi Sara,

Thanks for getting back to me. I am not allow to share to much but this is what is called and Active Electrical Cable (AEC) for QSFP. I see you pointed out that the VDDDSI pin but my email shows VSSSDI which should be VSSDSI. My mistake.

DAndr.6
Associate II

So my question is what should be done with the VSSDSI pin when DSI is not used?

Sarra.S
ST Employee

Hello again @DAndr.6​,

As it is clearly stated in RM0432 paragraph 5.1.4, if DSI functionality is not used at all, then VSSDSI pin must be grounded

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.