2023-01-18 06:54 AM
2023-01-19 08:49 AM
Hello @DAndr.6,
Your question is not really clear, what designs are we talking about ?
but the Ref man clearly states :
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-19 10:30 AM
Hi Sara,
Thanks for getting back to me. I am not allow to share to much but this is what is called and Active Electrical Cable (AEC) for QSFP. I see you pointed out that the VDDDSI pin but my email shows VSSSDI which should be VSSDSI. My mistake.
2023-01-19 10:57 AM
So my question is what should be done with the VSSDSI pin when DSI is not used?
2023-01-20 12:54 AM
Hello again @DAndr.6,
As it is clearly stated in RM0432 paragraph 5.1.4, if DSI functionality is not used at all, then VSSDSI pin must be grounded
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.