cancel
Showing results for 
Search instead for 
Did you mean: 

nucleo stm32h755 has a faulty stlink charging circuit

Ruồi
Associate III

I accidentally disabled the 3v3 pin on CN8, so now my Nucleo h755 board can no longer load the code.

In this case is there a way to save?
Thanks,

2 REPLIES 2
AScha.3
Chief II

What you "disabled " on pin header ?

AScha3_0-1721376334989.png

+

For flash the code, st-link is connected on CN1 , and powers also the H755 .

So check JP2 :

AScha3_1-1721376494592.png

 

If you feel a post has answered your question, please click "Accept as Solution".

I connected pin 3v3 on CN8 to pin GND.\

STLINK is still alive but STM32H755 can no longer be seen.