cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-H753ZI board's ADC1/2 ADC3 channel Index with GPI/O Pin assignments

RongShengWang
Associate III

Hi,

    Could you list NUCLEO-H753ZI board's ADC1/2 ADC3 channel Index with GPI/O Pin assignment table with the connector name / pin index on the board, using channel number as the index

    It is very difficult to configure CUBEMAX-ADC without this Table. Especially, some ADC pin(s) may not be accessible on this board. I appreciate if you can provide this table: 

   ADC1/2  Example

   Channel Index     GPIO    NUCLEO Board Connector Index     Connector Pin Index       Sharing Info

        IN3                   PA6            CN8-D12                                       (Pin 7)                                with ADC3_IN12 

 

  ADC3 Example

 Channel Index     GPIO    NUCLEO Board Connector Index     Connector Pin Index         Sharing Info

        IN2                PA2_C               CN8-A2                                            Pin 9                          with ADC1/2_IN14

 

Thanks,

Rong

1 REPLY 1
Amel NASRI
ST Employee

Hi @RongShengWang ,

Where exactly do you suggest to have such information?

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.