2024-05-31 06:18 AM
Hi ,
Does project files compiled and created in NUCLEO-H753ZI require any modification or recreation of project files when ported to STM32H743ZI.
2024-05-31 08:36 AM
Hello @senra and welcome to the ST Community :smiling_face_with_smiling_eyes:.
The difference between both STM32H743ZI and STM32H753ZI is the Crypto part. So, if you have a project on the STM32H753ZI without a Crypto implementation, you can migrate it to the STM32H743ZI without a problem.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-31 08:53 AM
Is the NUCLEO-H743ZI2 (MB1364B, ST-LINK/V3) really NRND? I see the NUCLEO-H743ZI (MB1137, ST-LINK/V2-1) one is, and that's not surprising, but the ZI2 doesn't have it's own landing page https://www.st.com/en/evaluation-tools/nucleo-h743zi.html
As I recall the STM32H753ZI is based on the ZI2 (MB1364B) board, so there's going to be a handful of different pins related to LEDs and QSPI, as I recall. https://www.st.com/en/evaluation-tools/nucleo-h753zi.html
There's a USE_XYZ type define to select between the board designs at the NUCLEO.H level
2024-05-31 08:57 AM
Hello @Tesla DeLorean
The NUCLEO-H743ZI2 is an NRND product:
The NUCLEO-H743ZI is an Obsolete product:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.